Other Parts Discussed in Thread: CONTROLSUITE
Hello Everyone,
Happy new year to all,
I have two questions,
1) Can anyone please let me know the exact evaluation board for the below requirement of BLDC motor drive,
BLDC motor driver for 12V to 60V DC - HALL Sensored based
Description : Voltages 12V to 60V
Current limiting at : 30A
Actual requirement: BLDC motor drive with,
a) over voltage protection
b) under voltage protection
c) over current shut
d) current limiting
e) motor direction change
f) brake
g) enable/disable
h) reverse polarity protection
i) lock rotor protection
j) temperature protection
k) supply wire short protection (optional)
l) both the directions should have same current and speed
m) over load protection
n) pwm output for speed info
Commutation type: Trapezoidal commutation
Method of commutation: Sensored or sensorless any
2) I read "Trapezoidal commutation gives better torque at lower speeds but no FOC" Please correct me if I am wrong.
Awaiting for the replies on both the questions.