This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD28335: CCS/TMS320F28335

Part Number: TMDSCNCD28335

Tool/software: Code Composer Studio

Good Afternoon everyone,

I am currently trying to flash some code into the flash memory of the TMDSCNCD28335. As such, I am currently trying to use the BlinkingLED example on the Resource Explorer. I have noticed that there is also an example on flashing on the Resource Explorer as well, but I have not had any successes on trying to merge the code together.

I have also taken notice of this chunk of code :

memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (Uint32)&RamfuncsLoadSize);

which, copies time critical code and flash setup code into the RAM of the device that I am using. However, once I start building and loading the code in, this error occurs :

C28xx: File Loader: Verification failed: Values at address 0x04000@Program do not match Please verify target memory and memory map.

I have searched online for details and more information on memory mapping, but am unsure of where and how to begin. Any help would be very very much appreciated