This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK28379D: Code does not execute if CCS is not connected

Part Number: TMDSDOCK28379D

Hi,

I'm new to the whole TI family and I'm running into some basic issues with learning the platform.

Should the C200Ware examples for the board be fully engineered to be run as standalone? Let's pick the "timed_led_blink_cpu01" project as an example. It runs fine if I'm loading it from CCS, but if I cycle power and disconnect my XDS110 probe, nothing happens. I have tried both flash and ram options.

If the examples are not ready for this purpose, what do I need to do at this point? I have read that the GEL file does something to set things right when the emulator and CCS is connected, but the forum posts seem to go cold and old pretty fast. Any updated resources I should be reading to solve this?

Best regards,

Tero