Part Number: TMS320F28035
Other Parts Discussed in Thread: AFE031
1) Is the "full" API of the PLC-Lite Modem software in the "PLC Lite Host Message Protocol Specification"?
2) Is it possible to add application code to the DSP next to the PLC-Lite driver or do I need to add another micro-controller that talks via de Host protocol to the PLC-Lite software?
3) Is there any other information the host protocol can get from the modem like collisions?
4) Can I use broadcasting with PLC-Lite
Beste regards,
R