Part Number: TMS320F28054M
Other Parts Discussed in Thread: MOTORWARE
Tool/software: Code Composer Studio
I have developed a custom low voltage drive board using TMS320F28054M. While implementing lab2b of motorware, to detect motor parameters, I found out that the resistance value of a motor which is in the range of 0.3 ohms, keeps coming within 0.32 to 0.48 which is too wide a variation, however, the motor runs well if I use value in the range of 0.3 to 0.35 the motor runs well in lab3 and above, a resistance value above that trips the motor if I try to run forward / reverse quickly. The motor current, terminal voltage etc in CCS and actually measured look in tune. Also I checked if there is any ripple on the current feedback and apparently it looks quite low. In view of this somebody can guide me what might be going wrong for resistance detection and how can I check the same?