Hello,
new to C2000,
if running out of pins, can I use comparator in PGA1_IN/CMP1_LP2 to measure frequency input (8KHz)?
if Yes, can provide the details internal connectivity required?
Thanks.
CK
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
new to C2000,
if running out of pins, can I use comparator in PGA1_IN/CMP1_LP2 to measure frequency input (8KHz)?
if Yes, can provide the details internal connectivity required?
Thanks.
CK
CK,
Yes, you can use the CMPSS through its input MUX on PGA1_IN to extract digital high and low transitions from the sensor. The ECAP can process the CMPSS output transitions by configuring its input selection MUX (which is different from the Input, Output, and ePWM X-BARs).
-Tommy