Other Parts Discussed in Thread: UNIFLASH, LAUNCHXL-F28069M
Tool/software: Code Composer Studio
I am using XDS100v2 usb emulator for debugging and programming of TMS320F28069M device.
In some o the boards there is no problem in programming and debugging but in some of the boards I get the following result:
Error connecting to the target:
(Error -1135 @ 0x0)
The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation.
(Emulation package 6.0.628.3)
Also in one of the boards I can read and program the device with Uniflash but it is not possible with Code Composer Studio.
I am confused and it is hard to understand why does that such a problem occur in some of the boards? (The components and schematic is exactly the same for all boards)
Best regards