Part Number: SM320F28335-HT
I have some questions and I will be very pleased if anyone can help me with them:
1- What is the temperature range of this IC?
2- Is the IC mounted on a card or it is standalone. If yes, what is the temperature range for the card?
3- Is the card have an interface board. If yes, what is the temperature range for the interface board?
Thanks a lot