This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28035: SPLL_1ph_SOGI

Part Number: TMS320F28035
Other Parts Discussed in Thread: CONTROLSUITE

Tool/software: Code Composer Studio

Hi TI experts,

I have copied SPLL_1ph_SOGI example code from the solar library into my project to do PLL.

My questions are:

(1) It is sort of working, but I found that the estimated voltage has some delay (3 cycles if 10kHz) compared the measured one. Is it expected due to the filter? What parameters may affect this?

(2) Is there a TI example project in the ControlSuite or anywhere that uses the SPLL_1ph_SOGI? If so, I can download the example project to see if I have made something wrong.

(3) Any parameters I may need to change to adjust to my project? If my sampling frequency is 10kHz, instead of 20kHz, what parameters do I need to change, and any quick guide one how to calculate it?

Thank you in advance.