Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE, CONTROLSUITE
Hi,
I've integrated VCU CRC8 library from C2000Ware 1.00.03.00 package into my CCS project. I am intending to generate a CRC8 of the bytes in a CAN message. And yes, I know CAN already does a CRC for the message.
Anyway, I've used the examples in the C2000Ware_1_00_03_00_Software\libraries\dsp\VCU\c28\examples\crc\2837x_vcu2_crc_8 project and implemented them in my codebase.
I am only trying to generate CRC8 on 8 bytes. I have found that for the VCU, the bytes need to be packed into uint16_ts. I've confirmed that the CRC8 is correct and I am happy with the data.
What is really troubling me, is that it takes over 8ms to generate a CRC8 if using assembly based functions and even longer if using C based functions. I am only generating CRC8 on 8 bytes, 4 words. Please see my configuration below:
/**
* CRC object initialisation. No buffer or byte count as they will differ per CAN message.
*/
static void can_init_crc(void) {
/* Step 1: Initialize the CRC object */
CRC.seedValue = INIT_CRC8;
CRC.nMsgBytes = 0;
CRC.parity = CRC_parity_even;
CRC.crcResult = 0;
CRC.pMsgBuffer = 0;
CRC.pCrcTable = (uint16_t*)&crc8Table[0];
CRC.init = (void (*)(void*))CRC_init8Bit;
CRC.run = (void (*)(void*))CRC_run8Bit;
/* Step 2: Initialize the handle */
handleCRC = &CRC;
/* Step 3: Run the 8-bit table look-up CRC routine and save the result */
CRC.init(handleCRC);
}
/**
* Function to calculate CRC* on the given payload array.
*
*/
static inline uint16_t can_calc_crc(uint16_t* payload, uint16_t dlc) {
uint16_t resp = 0U;
uint16_t packed_payload[4U] = {0};
uint16_t wordIdx = 0U;
/**
* Pack each byte in payload into continuous data LSBMSB format
* payload[n] -> packed[word](LSB)
* payload[n+1] -> packed[word](MSB)
*/
for(uint16_t id = 0U; id < dlc; id += 2) {
packed_payload[wordIdx] |= (payload[id]);
packed_payload[wordIdx] |= (payload[id + 1] << 8);
wordIdx++;
}
CRC.pMsgBuffer = packed_payload;
/* -1 to not include the CRC byte in calculation */
CRC.nMsgBytes = dlc - 1;
CRC.run(handleCRC);
resp = (uint16_t)CRC.crcResult;
CRC.crcResult = 0;
return (resp);
}
Using oscilloscope and some GPIO toggling, I can see that the "can_calc_crc" function takes 8ms to return. Is this normal? Is there some flag that I need to enable the VCU explicitly? I am using VCU2 and the library included is "c28x_vcu2_library_fpu32.lib"
Kind regards.