This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C28346: BSDL File Problem

Part Number: TMS320C28346

Hi,

When loading the BSDL file for the TMS320C28346 (sprm424) into our BSDL environment, the software gives the following warning:

Invalid pin name VSS on component Device 1 (M:\Boundary Scan\BSDL Model\TMS320C28346ZFE (sprm424).bsm)


When viewing into the BSDL file I can see that in the following lines there are no valid ball names (bold lines):

  "GPIO0   :  D2," &
  "GPIO1   :  E1," &
  "VSS        :  VSS," &
  "VSSK    :  A8," &
  "VDDIO     :  VDDIO," &
  "VDD        :  VDD," &
  "GPIO2   :  E2," &

How should I edit the file to get no warning? Can I just delete those three lines?

Thanks and best regards,

Patrick