This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/C2000-GANG: ERROR 70: DSP CLK frequency error

Part Number: C2000-GANG
Other Parts Discussed in Thread: TMS320F28027

Tool/software: Code Composer Studio

Hi,

I have tried for first time the C2000-GAN programmer in our custom designed board (MCU TMS320F28027 running at 60MHz from internal clock). I am using the "Interactive Mode", as it is recommended for first time users in SPRUHS0C. I have generated, I think correctly, the .hex file in Code Composer (Properties -> Build -> C2000 HEX Utility -> Output Format Options):

- When I press "GO (F9)", the process Fail in the step 6. The software shows the following error message: "ERROR 70: DSP CLK frequency error". In the OSC textbox, I see 2.49 - 2.49, and in SYS textbox I see 7.50 - 7.50.

Note: I am able to program my target without errors using the XDS110 and the application runs well.

Does anybody know the cause and solution to this error? 

Thank you in advance.

Ramon Navarro