Part Number: TMS320F28377D
Dear All:
I use the TMS320F28377 to design the Servo controller, i have run into some problems in my design, and i need your help. The problems are as follows:
1. the jtag PIN2 can't pull to 0V, the PIN2 is only 2.3V
2. the ram can download programs, but the FLASH can't
3. the ram can download programs, but it can't run,show “low power mode”
can you help to resolve the problems? Thanks~