Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Hi, I am working on tms320f28377s microcontroller which is going to be integrated into an inverter circuit. However, some other guy designed the PCB for the microcontroller die which has only the I/O pins, JTAG, an unconnected 6-pin IC and a lot of pads on it. The PCB looks very similar to the one attached here:
However, there is no power supply to the PCB at all! And the XDS100V3 programmer manual says that it cannot power the micro-controller. So now, I have to design the power supply and I am having a very tough time. How do I solder the existing PCB onto the power supply PCB? The only way I can supply power to different pins is through pads provided on the PCB. Or do I solder wires out of these pads and connect it on a breadboard and supply power?
Please help! I am stuck!