Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Hello,
I have a question on an example ccs project of the controlSUITE software package.
Specifically I have a question on the following ccs project: controlSUITE>device_support>F2837xS>v210>F2837xS_examples_Cpu1>cla_matrix_mpy
I have built the ccs project and executed it in the debug environment.
I have included the screen capture display of the execution result.
After the execution has been done, the values of the pass and fail variables are still zeros.
They should be pass=9 and fail=0 if the project were executed correctly.
Through some tests, I have found out that the program flow does not exit from the function of Cla1ForceTask1andWait().
In addition, I can not figure out why the status of CPU1_CLA1 is displayed as (Disconnected : Unknown) even though the status of C28xx_CPU1 is displayed as (Running).
Thank you for your guidance.
With regards,
G. Kim