Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hello,
I am using TMS320f28069 control card . I have taken the "Example_2806XAdcSoc" example code . ADC is of 12 bit resolution (ie 4095 at 3.3 v).
1. Whenever I am connecting the ADC input pin to Ground pin of the docking station i am getting 0 in the result register , but when i am connection the input pin of ADC to 3.3 v the output count is fluctuating from 4095 to sometimes 4093 . I am not sure why is this happening ?? P.S I have used the ground and 3.3 v pin from the docking station.
2. Also if I am not using the ADC offsert calibiration function the output register fluctuates for both ground as well as 3.3 V . So plz let me know if the use the offset calibration function is necessary ??
3. Also why is it needed to calibrate the ADC each time we run the code . Accoding to me if once we did the calibration next time it should not be required to calibrate the ADC again .
Please let me know reasons for this strange behaviour , if any other steps is needed to be done.
I have read the post "e2e.ti.com/.../587441 " but it is still not clear why the value is fluctuating . Also i cannot under the nned of calibration every time .
Thank you
Rohit Sawa