Part Number: SM320F28335-HT
Other Parts Discussed in Thread: TMDSCNCD28335,
Hi There
i'm looking at using the SM320F28335-HT for a high temperature motor application, i already have the TMDSCNCD28335 plug in module and TMDSHVMTRPFCKIT motor dev kit. The issue i have is thaat i'd like to interface to a 24V motor. (note, its unopened and i will send it back if not suitable)
Question 1) can i simply supply TMDSHVMTRPFCKIT with 24V DC? (i know its HV but the literature doesn't specify a minimum voltage.
question 2) if the above isn't possible can can i buy a DRV8301-69M-KIT and simply change the card (from the TMDSCNCD28069MISO to the TMDSCNCD28335)? or is there lots of modifications i would need to make?
Kind Regards