Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: DRV8305, DRV8323, MOTORWARE
Hi,
in the past i have tested all the instaspin labs with the F28069M LP and DRV8305 boosterpack without any problems, including instaspin FOC and instaspin MOTION.
Recently I have tried to switch over to the DRV8323 Boosterpack, but have had trouble duplicating the Lab 5B as an example.
The additional Instaspin code files for the DRV8323 boosterpack came from the DRV8323 product folder, and I added them to motorware.
Since the DRV8323 Boosterpack connectors are connected slightly differently with regard to Phase Current and Phase Voltage as compared to the DRV8305, I doublechecked the mapping of ADC channels to current and voltage rails, and validated that the hal.c for DRV8323 is correct, so I don't think it is an ADC mapping issue.
Teknic_M2310PLN04K motor is used.
The motor phases are connected like the DRV8305, i.e. Mot A/B/C. VM power supply is 19.5V for this test from a notebook power supply.
user_j1.h variables are default for the Teknic_M2310PLN04K motor.
When the motor starts, it goes into its ONLINE state, it tries to spin but the velocity is not controllable.
The DRV8323 does not show the fault condition during this test.
Could you tell me if we have validated the DRV8323 with instaspin labs, like lab 5B?
Please let me know your thoughts.
Thanks,
--Gunter