Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: SN65HVD234, LAUNCHXL-F280049C
All:
The LAUNCHXL-F28379D has a CAN transceiver (SN65HVD234) that goes to a 2-pin header + ground.
If I wanted to experiment with CAN, could I connect two Launchpads by connecting CANH to CANH, CANL to CANL, and ground to ground?
Each Launchpad would have transceivers and it looks like it would also have the required 120 Ohm termination.
I tried searching and I could not see a post with this - any problems, if I keep the distance between Launchpads close, and use 3 jumpers?