Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I have read some of the e2e threads on similar issues, but still wanted to summarize what I am running into when trying to use the serial flash programmer.
Right now the cmd output is stuck here:
C:\temp>serial_flash_programmer.exe -d f2806x -k C:\temp\f28069_flash_kernel.txt -a C:\temp\Example_2806xLEDBlink.txt -p COM9 -w -v
C2000 Serial Firmware Upgrader
Copyright (c) 2013 Texas Instruments Incorporated. All rights reserved.
getting comm state
building comm DCB
adjusting port settings
calling f05_DownloadImage
Downloading C:\temp\Example_2806xLEDBlink.txt to device...
Here is what I have done, could you look through this and let me know if I am missing something?
[] Using Controlsuite v3.4.7 and serial_flash_programmer from that, unmodified
[] Using LED blink example build for FLASH mapping. Validated that it runs fine from Flash on F28069M LP, in GET_MODE boot.
[] LP bootmode is set for SCI boot
[] LP J7 MUX_SEL is ON, J6 CH_SEL is OFF, this should lead to UART RX/TX pins being available on J5.3/J5.4
[] LP J5.3/J5.4 are connected to FTDI cable RX/TX pins, and GND is connected as well
[] PC enumerates the COM port here on COM9
[] Before running the above command, I am giving the LP a push button reset
Is there anything else I am missing?
Unfortunately I currently cannot use the existing Visual Studio project, as I only have VS 2010, and there are some other issues with that currently.
Thanks,
--Gunter