Part Number: TMS320F28335
Dear all,
One of my AA has to implement the boundary scan through JTAG controller.
In a note of the BSDL file of the TMS320F28335, it is written that :
F33x Devices have two taps - one for the CPU and one for the boundary scan.
The bounday scan IR size is 3 bits.
Whhat does it mean ? Are 2x BSDL file required ? or are the TAPs transparent for the user ?
Moreover in order to enter in boundary scan test the following configuration must be used:
EMU1 = 0;
EMU0 = 1
XRSn = 1
TRSTN = 0 to 1
On the bord TRST is pulled down, does the 0 to 1 transition will be automatically happen at power up of the board ?
regards,
Domenico