Part Number: TMS320F28069
Other Parts Discussed in Thread: CONTROLSUITE
Dear Friend,
I am trying to use the Analog comparator for comparing the external analog voltage with the reference voltage and then the output of the comparator has to to be captured for high capture module. I tried to use EPWM TZ (trip zone ) sample program provided in the Control Suite software.
When I am trying to use ADCA2, and ADCB2 as signals as comparator input. Is the output of comparator starightway cannot come to GPIO 20 (Comparator output)?
When I am checking the comparator output at GPIO 20 pin , I am not getting any change if i swap the ADC1 & ADC2 signals. IS there any sample program or application note to understand ?
Kindly indicate where am I making mistake?
Regards,
S.M.Sundari,