Part Number: TMS320F28377D
Other Parts Discussed in Thread: AMC1305L25, C2000WARE
Tool/software: Code Composer Studio
Hi community
- Could anyone please help me in determining the accuracy of my sensor board?
In this board, AMC1305L25 IC is used with a shunt resistor (0.0015 ohm). I wonder if somebody please let me know what is the lowest value of current variation that this sensor could detect if I use Sinc3 and OSR=X with ENOB=Y bits.
- Is it possible to increase the accuracy by using higher value shunt resistor?
- In order to increase the accuracy, if i'm sure that my current is such small that the input voltage of AMC would stay in its linear range, could I use lower bit shifts than the one proposed in table 12-5 TRM ? for example is it possible to use 3 shifted bits for OSR=63 instead of 4-bit shift? Is it an effective way to increase the lowest value of the current variation detected by the sensor?
regards