This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-F280049C: Error Connecting during debug

Part Number: LAUNCHXL-F280049C

Tool/software: Code Composer Studio

I am attempting to run the blinky led example program from c2000 for my F280049C LaunchPad.

I am running CCS version 8.3.0.00009.

The program complies without issues.

But when I attempt to debug I receive an "IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0)…" in the console window.  I also get the same message in a popup dialog.

At first, I thought the issue was the emulation package issue reported earlier.  So I downgraded my emulation package to 8.0.803.0.  Loaded the firmware and verified I have version 2.3.0.15 on the board.

No joy.

I did verify the standalone program that came with the launchpad works and connects to my terminal emulation program without issues.

Any suggestions would be appreciated.

Thanks!

Brett