Part Number: TMS320F28375D
I just wanted to confirm that I can configure the X-BAR to use GPIO41 as an interrupt on a TMS320F28375D processor.
The X-BAR documentation says it can configure any GPIO pin, but in the Technical Reference manual GPIO section (7.2 number 1) it says that GPIO41 is hard-wired to be the wake-up signal in hibernate mode. I don't plan on using the hibernation feature, so I don't need to worry about using the wake-up signal.