Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hello,
My application works fine when i am running it through RAM, but when I am running it through flash variables in .ebss section are getting corrupted eg. i have one array of size 34 a[34], in application i only use data at locations a[0],a[1],a[2],a[3], but when i start debugger i get garbage data at locations a[5] to a[33] instead of zero. This is the case with all arrays i have defined. is there any problem with linker file? or what could be possible reasons
Please find my linker file below.
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode */
BEGIN : origin = 0x0A0000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x002000
// RAMLS1 : origin = 0x008800, length = 0x000800
// RAMLS2 : origin = 0x009000, length = 0x000800
// RAMLS3 : origin = 0x009800, length = 0x000800
// RAMLS4 : origin = 0x00A000, length = 0x000800
RAMGS14 : origin = 0x01A000, length = 0x001000
RAMGS15 : origin = 0x01B000, length = 0x001000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH_J : origin = 0x0A0002, length = 0x017ffe /* on-chip Flash */
// FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
// FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
FLASHO : origin = 0x0C0000, length = 0x002000 /* on-chip Flash */
FLASHP : origin = 0x0C2000, length = 0x002000 /* on-chip Flash */
FLASHQ : origin = 0x0C4000, length = 0x002000 /* on-chip Flash */
FLASHR : origin = 0x0C6000, length = 0x002000 /* on-chip Flash */
FLASHS : origin = 0x0C8000, length = 0x008000 /* on-chip Flash */
FLASHT : origin = 0x0D0000, length = 0x008000 /* on-chip Flash */
FLASHU : origin = 0x0D8000, length = 0x008000 /* on-chip Flash */
FLASHV : origin = 0x0E0000, length = 0x008000 /* on-chip Flash */
FLASHW : origin = 0x0E8000, length = 0x008000 /* on-chip Flash */
FLASHX : origin = 0x0F0000, length = 0x008000 /* on-chip Flash */
FLASHY : origin = 0x0F8000, length = 0x002000 /* on-chip Flash */
FLASHZ : origin = 0x0FA000, length = 0x002000 /* on-chip Flash */
FLASHAA : origin = 0x0FC000, length = 0x002000 /* on-chip Flash */
FLASHAB : origin = 0x0FE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2_8 : origin = 0x00E000, length = 0x008000
/* RAMGS3 : origin = 0x00F000, length = 0x001000
RAMGS4 : origin = 0x010000, length = 0x001000
RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000*/
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
RAMGS12 : origin = 0x018000, length = 0x001000
RAMGS13 : origin = 0x019000, length = 0x001000
}
SECTIONS
{
/* Allocate program areas: */
codestart : > BEGIN PAGE = 0, ALIGN(4)
.cinit : > FLASHH_J PAGE = 0, ALIGN(4)
.pinit : > FLASHH_J, PAGE = 0, ALIGN(4)
.text : > FLASHH_J PAGE = 0, ALIGN(4)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMGS2_8 PAGE = 1
.esysmem : > RAMLS0 PAGE = 0
.cio : > RAMLS0 PAGE = 0
/* Initalized sections go in Flash */
.econst : > FLASHH_J PAGE = 0, ALIGN(4)
.switch : > FLASHH_J PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
/*
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHM,
RUN = RAMD0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3|RAMLS4,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
*/
.TI.ramfunc : LOAD = FLASHH_J,
RUN = RAMLS0 | RAMGS14 | RAMGS15,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
ramgs0 : > RAMGS0, PAGE = 1
ramgs1 : > RAMGS1, PAGE = 1
/* /* The following section definitions are for SDFM examples */
/* Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333*/
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/