This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Compatibility with BOOSTXL-SHARP128

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: BOOSTXL-SHARP128

Hello,

In the BoosterPack Checker, I could find that the BOOSTXL-SHARP96 is compatible with the LAUNCHXL-F28379D.

However, on the product page of this booster, it is stated that the product is obslete and replaced by the BOOSTXL-SHARP128 version.

But the checker doesn't provide any information regarding that booster, I believe they are pin to pin compatible and that the booster is compatible with the launchpad as well but wanted an official confirmation.

Clément