Hi
I am facing problem using ADC of the 28335 board.I bult a simple model in simulink, to read the value of ADC input into a memory location and store it into a variable.
Now, when i execute the program and with no input to the ADC pin (ADCBIN0 in my case), the value of the corresponding input is not showing zero, but some arbit value. Even the corresponding ADCRESULT register is showing some arbit value.
Can someone please tell me whats the problem and how to intialize the ADC registers from SIMULINK ( if thats the problem of error).
Guess this is a basic "starters" problem and so i am awaiting a reply soon.
Thanks in Advance
Vijay Chand Ganti.