Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: CONTROLSUITE
I have been using the preflashed code on my f28035 controlCard to spin a motor with this motor control kit. I'd like now to try using the supported BLDC_Sensored code found in the folder C:\ti\controlSUITE\development_kits\DRV8312-C2-KIT_v128\BLDC_Sensored. Inside this BLDC_Sensored folder, there are a number of files. My understanding is that the code that is preflashed on the controlCard is a .out file, and I do not see any .out files in this folder. Which file do I need to flash to my controlCard? Also, will I be able to continue using the same GUI I have been with the preflashed code or will I have to do something differently?