Part Number: TMS320F28035
Hi,
I was surprised when I noticed that datasheet says 64KB of flash while the online description says 128KB flash.
Which one is correct?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
Hi,
I was surprised when I noticed that datasheet says 64KB of flash while the online description says 128KB flash.
Which one is correct?
Figures in the datasheet are given in units of "words", one word being 16-bits. This is because the device memory architecture is 16-bits.
However for easier comparison with other devices, the online device summary table lists memory in "bytes", i.e. 8-bit units.
64kW = 128kB, so actually these figures are the same.
Regards,
Richard