Other Parts Discussed in Thread: SFRA
Tool/software: Code Composer Studio
Hello, Manish. We work with SFRA project _IQ , F28035. Only SFRA. We got good stable plant, test it , all OK. DC Voltage is controlled very stable. Thank you much for your advices. But , when we launch AC on this board - it gives very good sine if open loop, But when we insert 3P3Z coefficients which we got for DC ( the board, all inductives, and capacitors are the same - all the board is the same-project HV_SOLAR_DC_AC) , so when we try to control AC through these coefficients we can not get even normal sine form. We control Voltage. Question : are coefficients which are good for DC are good for AC? (Concerning the same topolgy) And how it is possible to make a sine which is getting through 24 kHZ PWM with filter (3P3Z - in real 2P2Z) which has the bandwidth only 1.5 kHZ? Again - HV_SOLAR_DC_AC - excelent sine when open loop. Not sine at all - when 2P2Z ( Voltage control). PWM rate is 24 kHZ, control rate the same 24 kHz. Voltage control. DC vs AC.