Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE
Hi,
The TRM discusses the HRPWM configuration and the notion of MEPs. It has been said that the duration of 1 MEP is about 150 picoseconds. However if mu MCU is running at 90Mhz then 1 SYSCLK is 11.1ns long and from there the 150 picosecond period is about 1/74-th. Thats an odd number and from there I assume that actually the MEP is 1/64-th of SYSCLK as 64 can be described with 6 bits?
From this I assume that while the TBPRDHR register is 16 bits long, then only upper 6 bits are relevant and remaining 10 bits are unused? That would give 64 microsteps fro every SYSCLK and the 1 MEP duration would be about 174 picoseconds at 90Mhz operation.
Is that correct?