Part Number: TMS320F28377D
Other Parts Discussed in Thread: TMS320F28335, , C2000WARE
Tool/software: Code Composer Studio
Hello everyone
I'm recently upgraded myself from TMS320F28335 to TMS320F28377D and I'm newbie in dual core microcontrollers.
I loaded "gpio_ex1_setup" from "C2000Ware_1_00_01_00/driverlib/f2837xd/examples/cpu1/gpio/CCS/gpio_ex1_setup" into "CCSv8.1.0.00011"
and I added some additional code for togglling one LED on my custom board to the end of the main function as follows:
GPIO_setPinConfig(GPIO_91_GPIO91);
GPIO_setDirectionMode(91,GPIO_DIR_MODE_OUT);
while(1)
{
DEVICE_DELAY_US(300000);
GPIO_togglePin(91);
}
its works fine in the "CPU1_RAM" configuration, but when i click right on the project and choose "CPU1_FLASH" from "Bulid Configuration/Set Active/CPU1_FLASH" menu,
the erase and program process begin and complete sucessfully and by restarting board "turning board power supply off and then on" nothing happens and LED does not blink.
What i missed?
Any help will highly be appreciated.