Part Number: TMS320F28377D
Hi,
in spruhm8g.pdf, Section 4.4 of the TRM, it indicates that "In the case of a bulk DMA transfer to and from the same memory block the CPU is trying to access,
the arbitration will stall CPU access until the DMAcompletes single access, not the entire bulk transfer".
Now, I have a case,
DMA CH1/CH2/CH4 cpu1 cpu2 , they use the same EMIF,
DMA CH4 wants to transfer 160 words memory block,
Setting DMA BURST_SIZE=2, & TRANSFER_SIZE=80,
DMA CH1/CH2 cpu1 cpu2, they can not use EMIF when DMA CH4 working.
Is the above description right?
best regards,
Simen