Part Number: TMS320F28379D
Other Parts Discussed in Thread: CONTROLSUITE,
Tool/software: TI C/C++ Compiler
Hi,
The coder is not entering the ISR, What I am doing wrong ?
Any suggestion?
#include "F28x_Project.h"
void InitEQep1Gpio(void);
void InitEQep1(void);
__interrupt void EQep1_isr(void);
int Count;
int Loop_count;
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
InitGpio(); // Skipped for this example
CpuSysRegs.PCLKCR4.bit.EQEP1=1 ;
InitEQep1Gpio();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
// Map ISR functions
// Step 4. Initialize the Device Peripherals:
//
EALLOW;
PieVectTable.EQEP1_INT = &EQep1_isr;
EDIS;
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =0;
EDIS;
InitEQep1();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC =1; //Serve per sincronizzare gli interrupt
EDIS;
// Step 5. User specific code, enable interrupts:
// Initialize counters:
//
//
// Enable CPU INT3 which is connected to EPWM1-3 INT:
//
IER |= M_INT5;
//
// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
//
PieCtrlRegs.PIEIER5.bit.INTx1 = 1;
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global real-time interrupt DBGM
//
// Enable XINT1 and XINT2 in the PIE: Group 1 interrupt 4 & 5
// Enable INT1 which is connected to WAKEINT:
//
PieCtrlRegs.PIECTRL.bit.ENPIE = 1; // Enable the PIE block
IER |= M_INT1; //Enable group 1 interrupts
EINT;
for(;;)
{
Loop_count++;
}
}
__interrupt void EQep1_isr(void)
{
Count++;
//
// Clear INT flag for this timer
//
EQep1Regs.QCLR.bit.IEL = 1;
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP5;
}
void InitEQep1Gpio(void)
{
EALLOW;
//
// Disable internal pull-up for the selected output pins
// for reduced power consumption
// Pull-ups can be enabled or disabled by the user.
GpioCtrlRegs.GPAPUD.bit.GPIO20 = 1; // Disable pull-up on GPIO20 (EQEP1A)
GpioCtrlRegs.GPAPUD.bit.GPIO21 = 1; // Disable pull-up on GPIO21 (EQEP1B)
// GpioCtrlRegs.GPAPUD.bit.GPIO22 = 1; // Disable pull-up on GPIO22 (EQEP1S)
GpioCtrlRegs.GPAPUD.bit.GPIO23 = 1; // Disable pull-up on GPIO23 (EQEP1I)
//
// Synchronize inputs to SYSCLK
// Synchronization can be enabled or disabled by the user.
// Comment out other unwanted lines.
//
GpioCtrlRegs.GPAQSEL2.bit.GPIO20 = 0; // Sync GPIO20 to SYSCLK (EQEP1A)
GpioCtrlRegs.GPAQSEL2.bit.GPIO21 = 0; // Sync GPIO21 to SYSCLK (EQEP1B)
// GpioCtrlRegs.GPAQSEL2.bit.GPIO22 = 0; // Sync GPIO22 to SYSCLK (EQEP1S)
GpioCtrlRegs.GPAQSEL2.bit.GPIO23 = 0; // Sync GPIO23 to SYSCLK (EQEP1I)
//
// Configure EQEP-1 pins using GPIO regs
// This specifies which of the possible GPIO pins will be EQEP1 functional
// pins.
GpioCtrlRegs.GPAMUX2.bit.GPIO20 = 1; // Configure GPIO20 as EQEP1A
GpioCtrlRegs.GPAMUX2.bit.GPIO21 = 1; // Configure GPIO21 as EQEP1B
// GpioCtrlRegs.GPAMUX2.bit.GPIO22 = 1; // Configure GPIO22 as EQEP1S
GpioCtrlRegs.GPAMUX2.bit.GPIO23 = 1; // Configure GPIO23 as EQEP1I
EDIS;
}
void InitEQep1()
{
EQep1Regs.QUPRD = 2000000; // Unit Timer for 100Hz at 200 MHz
// SYSCLKOUT
EQep1Regs.QDECCTL.bit.QSRC = 00; // QEP quadrature count mode
EQep1Regs.QEPCTL.bit.FREE_SOFT = 2;
EQep1Regs.QEPCTL.bit.PCRM = 00; // PCRM=00 mode - QPOSCNT reset on
// index event
EQep1Regs.QEPCTL.bit.UTE = 1; // Unit Timeout Enable
EQep1Regs.QEPCTL.bit.QCLM = 1; // Latch on unit time out
EQep1Regs.QPOSMAX = 0xffffffff;
EQep1Regs.QEPCTL.bit.QPEN = 1; // QEP enable
EQep1Regs.QCAPCTL.bit.UPPS = 5; // 1/32 for unit position
EQep1Regs.QCAPCTL.bit.CCPS = 6; // 1/64 for CAP clock
EQep1Regs.QCAPCTL.bit.CEN = 1; // QEP Capture Enable
EQep1Regs.QEINT.bit.IEL = 1 ;
EQep1Regs.QEPCTL.bit.IEL = 1;
}