This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: (64pin) GPIO8 Outputs 1.6V for High ?

Part Number: TMS320F280049C

Hi,

I've got a new custom board with the 64pin TMS320F280049C.

I've got the hardware mostly running. I've got the clock, Uart, i2c all running fine.

But I'm stumped, GPIO8 when set up as an output and toggled, it only goes to 1.6V

Originally I had it set up as SPI MOSI and it worked with a few devices. But was giving me trouble

Are there any registers that can control this?

Cheers,

Alan