Part Number: TMS320F28335
In short: two TMS320F28335 communicate with SCI via RS485 on 9600 Hz. If the dividers of SCI differs on one point, framing error start happening really frequently. Clock generators are the same. One point of the divider is only 12 Hz in my case. What might be the problem?
I've got two devices with TMS320F28335 communicating with each other via RS485. If I set the same baud-rate devider on SCI on both MCU, everything works fine. Another device connected to the same bus operating on the same baud-rate provokes framing-error on my receivers with TMS320F28335.
I discovered that if I increase baud-rate devider on one point from 482 to 483 (baud-rate is 9600, 37.125 MHz slow peripheral bus clock rate) on one of my devices, framing error happens much rare on the frames from the other devices. But framing errors start happening on another of devices with TMS320F28335.
A osciloscope shows me not much differene between two close values of the divider.
Thank you in advance