Other Parts Discussed in Thread: TMS320F28379D
Tool/software: TI-RTOS
Dear support,
I have some problems with ti.platforms.tms320x28:TMS320F28076 project that built in: TI-RTOS ver2.16.1.14, XDSTools 3.32.2.25_core, Compiler TI v18.1.2_LTS.
Example project is attached
/cfs-file/__key/communityserver-discussions-components-files/171/7838.Test1.zip
1. When I download program to the card (DebugAs->Code Composer Debug Session) I get: "C28xx_CPU1: Error occurred during flash operation: Unknown property "FlashCoreSelection" error.
I work with C2000 Launchpad XL TMS320F28379D
2.get warning in the line: { -l F021_API_F2837xD_FPU32.lib} of cmd file
"Description Resource Path Location Type #10068-D no matching section TMS320F28076.cmd /Test1 line 118 C/C++ Problem
Could you pls help me to resolve these problems
Thanks,Sabina