Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE, LM311
Hi,
I'm trying to detect the zero crossing of two different 80kHz square waves using the F28379D. Once I read the zero crossing, I will make some decisions (set a GPIO and reset another).
I tried to use the ADC module, but it is too slow, and it causes too much delay. But I was told here in this forum that I could use the CMPSS module, but I can't find any exemples that I could use as a reference.
My question is: how fast the CMPSS module can be? Can I use the ADC ports to use this module?
Does anyone has a similar exemple or know where I can find one?
Thanks!