Part Number: TMS320F28379D
Dear Sir,
I need to trip all PWM signal as protection. For that, we are using the IGBT driver card signal. The output of the driver is a pulse train of 4uS to 10uS as per the protection level. I connected all the output to GPIO PINs of the controller.
Now the issue is how I identified the pulse width of input GPIO pin comes from the driver card.
Please guide me, is this possible using TRIP Zone and X-BAR Module? If yes please provide me the Outline/Steps to configure X-BAR and ePWM TRIP ZONE.
Ashutosh Bhatt