Part Number: TMS320F28069
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE
Hi people,
I need a solution how to bring a fully closed up unit (IP65) into Standalone Boot Mode (SCI) only by the use of a USB connection.
By the use of the exe file "serial_flash_programmer" I have managed to upload a new application code into my evaluation board:
serial_flash_programmer. exe -d f2806x -k f2806x_flash_kernel.txt -a CCS_LED_Test_1Hz.txt -p COM4 -b 9600 -w -v
To bring the eval-board into SCI boot mode I need to set GPIO34=1 and GPIO37=0 and the power up (reset).
On the eval-board setting up GPIO34 and 37 is done by the help of 2 DIP-switches and it works very fine!!
But.... how do I control if I want to go into boot mode or not without the use of DIP-switched?
Can I do something (write to some register) just before I reset the unit to get into Boot Mode.
I'll rather not have an extra hole in my IP65 cabinet for a DIP-switch.
Please help!