This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: Reset Circuit

Part Number: TMS320F28335
Other Parts Discussed in Thread: TPS3306

Hello,

I (My customer) would have questions on the reset of the DSP TMS320F2833X.

From the datasheet the minimum operating voltage of these devices is 3,135V, as in the image below

The reset supervision circuit should theoretically release the reset signal when the supply voltage rises above this minimum voltage.
The SLVA296A document prescribes the use of a TPS3306-18 which is a double supervisor because it controls both the VDD (3.3V) and the VDD core (1.8V).

See below please:

The threshold voltage of this supervisor is 2.93V for the VDD, which is lower than the minimum working voltage of the DSP.
Theoretically it does not seem correct, am I mistaking something?


Could it be that if there is a typical 100ms delay before the reset is released, is it counted that in that period of time the voltage VDD has "reasonably" reached its stability?
This is a particular situation in customer application where the VDD (and also the VDD core) are given very slowly and I would therefore like to clarify the doubts on the above questions.

Many Thanks,

Antonio

  • Antonio,

                 I reviewed the Reference Design and also the TPS3306 datasheet that you referred to. You are correct that the TPS3306 could potentially start deactivating the reset output when SENSE1 > 2.93v [but after a delay t(d)] and potentially before 3.135v, which is the Vmin for 2833x. Note, however, that the TPS3306 datasheet specs a MIN value of 70 mS for t(d). If the 3.3v supply ramps to at least 3.135v before the end of this period, then all is good.