Part Number: TMS320F28335
Hello everyone,
I want to program the card TMS320F28335 so that it can give as output two signals ePWM1X and ePWM2X. The isssue that I'm having is that these two signals are delayed with a value of 3.84us even if my program doesn't include this delay (I'm assuming it's a hardware issue). I used the deadband option in the ePWM bloc, which erased the delay from the "left" side of the pulse, while the one on the right remained. What are the solutions that I can implement in my program to fully get rid of this delay between the two signals ?
You can see below the two signals.