Part Number: TMS320F28035
Tool/software: Code Composer Studio
I am using TMS320F28035 SCI, in polling mode 115200 8 bit no parity mode without loopback.
I am getting the same data which I am transmitting one by one byte on SciaRegs.SCIRXBUF register.
I checked TX and RX are not connected physically and it works correctly when the other processor when I am sending data back and forth on TX/RX using other processor.
But when I removed the other processor free-ed up TX/RX lines. I am having this above issue.
Is the physical address of SCIRX and TX buffer the same ? How can I clear TX buffers after the data is transmitted ?
Thanks in advance.
signed int getchar(void)
{
signed int c = -1;
// if there are any unread characters in the FIFO, get the first-in
if (0 != SciaRegs.SCIFFRX.bit.RXFFST)
{
c = SciaRegs.SCIRXBUF.all;
}
else
{
c = -1;
if (0 != SciaRegs.SCIRXST.bit.RXERROR)
{
SciaRegs.SCICTL1.bit.SWRESET = 0;
SciaRegs.SCICTL1.all = 0x0023;
}
}
return(c);
}
Sci_init()
{
GpioCtrlRegs.GPAMUX2.bit.GPIO28 = 0; // function = GPIO
GpioCtrlRegs.GPAMUX2.bit.GPIO29 = 0; // function = GPIO
GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 2; // function = SCIRXDA
GpioCtrlRegs.GPAMUX1.bit.GPIO12 = 2; // function = SCITXDA
SciaRegs.SCICTL1.bit.SWRESET = 0; // Init SCI state machine
// FIFO
SciaRegs.SCIFFTX.all = 0xE040; // SCIRST | SCIFFENA | TXFIFOXRESET | TXFFINTCLR
SciaRegs.SCIFFRX.all = 0x605f;//0x2044; // RXFFIL = 15 | RXFFINTCLR | RXFIFORESET | RXFFOVRCLR
SciaRegs.SCIFFCT.all = 0x0; // Auto Baud disabled
SciaRegs.SCICCR.all = 0x0007; // Character len = 8
SciaRegs.SCICTL1.all = 0x0003; // TXENA | RXENA
SciaRegs.SCIHBAUD = 0;
SciaRegs.SCILBAUD = 15; // 48-38400 baud @LSPCLK = 15MHz
SciaRegs.SCICTL1.all = 0x0023; // TXENA | RXENA | SW RESET
EDIS;
SciaRegs.SCIFFRX.bit.RXFIFORESET = 0; // reset the FIFO pointer to zero
SciaRegs.SCIFFRX.bit.RXFIFORESET = 1; // re-enable receive FIFO operatio
}