Part Number: TMS320F28335
Tool/software: Code Composer Studio
hi all, this is my code of receiving float data in mailbox 1 .data which is receiving has a float value. i am not getting whats wrong in this program that it is not receiving float value.at transmitting side i convert float value in char type and send it to mailbox5
#include "DSP2833x_Device.h"
// external function prototypes
extern void InitSysCtrl(void);
extern void InitPieCtrl(void);
extern void InitPieVectTable(void);
extern void InitCpuTimers(void);
extern void ConfigCpuTimer(struct CPUTIMER_VARS *, float, float);
extern void InitECan(void);
// Prototype statements for functions found within this file.
void Gpio_select(void);
interrupt void cpu_timer0_isr(void);
//###########################################################################
// main code
//###########################################################################
char temp[6];
void main(void)
{
struct ECAN_REGS ECanaShadow; // local copy of CAN registers
//Uint16 temp;
InitSysCtrl(); // Basic Core Init from DSP2833x_SysCtrl.c
EALLOW;
SysCtrlRegs.WDCR= 0x00AF; // Re-enable the watchdog
EDIS; // 0x00AF to NOT disable the Watchdog, Prescaler = 64
Gpio_select(); // GPIO9, GPIO11, GPIO34 and GPIO49 as output
// to 4 LEDs at Peripheral Explorer
/* Initialize the CAN module */
// NOTE: first modify TI-file: InitECan() to 100kbps by setting BTR = 49
InitECan();
/* Write to Mailbox 1 message ID field */
ECanaMboxes.MBOX1.MSGID.all = 0x10000000; // extended identifier
ECanaMboxes.MBOX1.MSGID.bit.IDE = 1;
/* Configure Mailbox 1 as Receiver mailbox */
ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
ECanaShadow.CANMD.bit.MD1 = 1;
ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
/* Enable Mailbox 1 */
ECanaShadow.CANME.all = ECanaRegs.CANME.all;
ECanaShadow.CANME.bit.ME1 = 1;
ECanaRegs.CANME.all = ECanaShadow.CANME.all;
InitPieCtrl(); // basic setup of PIE table; from DSP2833x_PieCtrl.c
InitPieVectTable(); // default ISR's in PIE
EALLOW;
PieVectTable.TINT0 = &cpu_timer0_isr;
EDIS;
InitCpuTimers(); // basic setup CPU Timer0, 1 and 2
ConfigCpuTimer(&CpuTimer0,150,100000);
PieCtrlRegs.PIEIER1.bit.INTx7 = 1;
IER |=1;
EINT;
ERTM;
CpuTimer0Regs.TCR.bit.TSS = 0; // start timer0
while(1)
{
while(CpuTimer0.InterruptCount == 0);
CpuTimer0.InterruptCount = 0;
EALLOW;
SysCtrlRegs.WDKEY = 0x55; // service WD #1
EDIS;
if(ECanaRegs.CANRMP.bit.RMP1 == 1 ) // valid new data in MBX1?
{
*temp = ECanaMboxes.MBOX1.MDL.byte.BYTE0; // read message
ECanaRegs.CANRMP.bit.RMP1 = 1; // clear the status flag RMP1
// and prepare MBX1 for next receive
/*if(temp & 1) // update LED LD1
GpioDataRegs.GPASET.bit.GPIO9 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO9 = 1;
if(temp & 2) // update LED LD2
GpioDataRegs.GPASET.bit.GPIO11 = 1;
else
GpioDataRegs.GPACLEAR.bit.GPIO11 = 1;
if(temp & 4) // update LED LD3
GpioDataRegs.GPBSET.bit.GPIO34 = 1;
else
GpioDataRegs.GPBCLEAR.bit.GPIO34 = 1;
if(temp & 8) // update LED LD4
GpioDataRegs.GPBSET.bit.GPIO49 = 1;
else
GpioDataRegs.GPBCLEAR.bit.GPIO49 = 1;*/
}
}
}
void Gpio_select(void)
{
EALLOW;
GpioCtrlRegs.GPAMUX1.all = 0; // GPIO15 ... GPIO0 = General Puropse I/O
GpioCtrlRegs.GPAMUX2.all = 0; // GPIO31 ... GPIO16 = General Purpose I/O
GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1; // CANA_RX
GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1; // CANA_TX
GpioCtrlRegs.GPBMUX1.all = 0; // GPIO47 ... GPIO32 = General Purpose I/O
GpioCtrlRegs.GPBMUX2.all = 0; // GPIO63 ... GPIO48 = General Purpose I/O
GpioCtrlRegs.GPCMUX1.all = 0; // GPIO79 ... GPIO64 = General Purpose I/O
GpioCtrlRegs.GPCMUX2.all = 0; // GPIO87 ... GPIO80 = General Purpose I/O
GpioCtrlRegs.GPADIR.all = 0;
GpioCtrlRegs.GPADIR.bit.GPIO9 = 1; // peripheral explorer: LED LD1 at GPIO9
GpioCtrlRegs.GPADIR.bit.GPIO11 = 1; // peripheral explorer: LED LD2 at GPIO11
GpioCtrlRegs.GPBDIR.all = 0; // GPIO63-32 as inputs
GpioCtrlRegs.GPBDIR.bit.GPIO34 = 1; // peripheral explorer: LED LD3 at GPIO34
GpioCtrlRegs.GPBDIR.bit.GPIO49 = 1; // peripheral explorer: LED LD4 at GPIO49
GpioCtrlRegs.GPCDIR.all = 0; // GPIO87-64 as inputs
EDIS;
}
interrupt void cpu_timer0_isr(void)
{
CpuTimer0.InterruptCount++;
EALLOW;
SysCtrlRegs.WDKEY = 0xAA; // service WD #2
EDIS;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;
}
plz, tell me what wrong in this?