Part Number: TMS320F28379D
Hi,
I use Fapi_issueAsyncCommandWithAddress() API to erase FLASH sectors. But, within cmd file, I have a different sector definition than the one defined in the default cmd files. For example, I have a sector which embraces all FLASH addresses corresponding to standard sectors from A to E. In that case, what is erased if I pass the standard FLASH A sector origin address to the API, only standard sector A or the whole sector I have defined in cmd file (standard sectors from A to E are erased)?
Also, in case I had defined all sectors as standard cmd file defines what would be erased if I passed an address from the middle of the A sector?
Thanks in advance!
Best regards,
Adria