Part Number: TMS320F28027
We're using the Piccolo Launchpad to read a digitized light level coming from a photodiode. The output from the photodiode is amplified by a PGA. We used similar hardware on an earlier project so I'm fairly confident that this hardware should be working okay.
Using the driver model, I'm having the PWM module trigger a conversion on A1 using channel 14. The ADC interrupt happens okay. In the ISR, I read the value output from ADC_ResultNumber_1, store it in a local variable, and notify a loop in my main() function that displays the value at non-interrupt time. The output value, however, is incorrect (never 0, but always far too low).
Here is the relevant code. Can anyone see anything that might be incorrect here?
void adc_init()
{
CLK_enableAdcClock(myClk);
ADC_enableBandGap(myAdc);
ADC_enableRefBuffers(myAdc);
ADC_powerUp(myAdc);
ADC_enable(myAdc);
ADC_setVoltRefSrc(myAdc, ADC_VoltageRefSrc_Int);
PIE_enableAdcInt(myPie, ADC_IntNumber_1);
CPU_enableInt(myCpu, CPU_IntNumber_10);
CPU_enableGlobalInts(myCpu);
CPU_enableDebugInt(myCpu);
// Configure ADC
ADC_setIntPulseGenMode(myAdc, ADC_IntPulseGenMode_Prior); // ADCINT1 trips after AdcResults latches
ADC_enableInt(myAdc, ADC_IntNumber_1); // Enable ADCINT1 interrupt
ADC_setIntMode(myAdc, ADC_IntNumber_1, ADC_IntMode_ClearFlag); // Disable ADCINT1 continuous mode
ADC_setIntSrc(myAdc, ADC_IntNumber_1, ADC_IntSrc_EOC1); // EOC1 trigger causes ADCINT1 interrupt to occur
ADC_setSocChanNumber(myAdc, ADC_SocNumber_1, ADC_SocChanNumber_B6); // SOC1 channel select = ADCINB6
ADC_setSocTrigSrc(myAdc, ADC_SocNumber_1, ADC_SocTrigSrc_EPWM1_ADCSOCA); // SOC1 start trigger = EPWM1A
ADC_setSocSampleWindow(myAdc, ADC_SocNumber_1, ADC_SocSampleWindow_7_cycles); // SOC1 sample/hold = 7 ADC clock cycles (6 ACQPS plus 1)
}
interrupt void adc_isr(void)
{
digitized_sample = ADC_readResult(myAdc, ADC_ResultNumber_1);
sample_ready = 1; // Notify main() loop for display
ADC_clearIntFlag(myAdc, ADC_IntNumber_1);
PIE_clearInt(myPie, PIE_GroupNumber_10);
return;
}