This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSDOCK28335: COM port is not detected in Device Manager

Part Number: TMDSDOCK28335
Other Parts Discussed in Thread: TMS320F28335

Hi,

when I plug in USB cable for TMS320F28335 Experimenter Kit, COM port is not detected in Device Manager.

I was trying to enable CAN communication and was doing some connections on the board so probably did something wrong as now I don't even have serial communication working. Even if I use another  controlCARD, it does not work.. so it think it must be an issue with this particular Docking Station. Because another pair of controlCARD and Docking Station is working fine.

Is there some test points to check if serial communication is still okay. I get all three diodes LD1, LD2 and LD3 on controlCARD working, SW1 is in OFF position and on Docking Station jumper is on J9 adn LD1 is ON, SW1 is in USB position. UBS port works also fine.

Regards.