Part Number: TMS320F28035
Hi,
I'm working on Over The Air firmware upgrade and I want to generate relocatable object file which can be placed in desired flash sector. Can any one help me with this...
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28035
Hi,
I'm working on Over The Air firmware upgrade and I want to generate relocatable object file which can be placed in desired flash sector. Can any one help me with this...
Thanks in advance.
try these options in linker -ar ( --absolute_exe and --relocatable).
Regards
Baskaran
Can you try to configure the address alignment in linker command file.
Also attach the current changes you did to device.h and also linker command file.
/*
//###########################################################################
//
// FILE: F2808.cmd
//
// TITLE: Linker Command File For F2808 Device
//
//###########################################################################
// $TI Release: F2803x C/C++ Header Files and Peripheral Examples V130 $
// $Release Date: May 8, 2015 $
// $Copyright: Copyright (C) 2009-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
*/
/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file,
// add the header linker command file directly to the project.
// The header linker command file is required to link the
// peripheral structures to the proper locations within
// the memory map.
//
// The header linker files are found in <base>\DSP2803x_Headers\cmd
//
// For BIOS applications add: DSP2803x_Headers_BIOS.cmd
// For nonBIOS applications add: DSP2803x_Headers_nonBIOS.cmd
========================================================= */
/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper
// locations within the memory map */
/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP2803x_Headers_nonBIOS.cmd */
/* Uncomment this line to include file only for BIOS applications */
/* -l DSP2803x_Headers_BIOS.cmd */
/* 2) In your project add the path to <base>\DSP2803x_headers\cmd to the
library search path under project->build options, linker tab,
library search path (-i).
/*========================================================= */
/* Define the memory block start/length for the F28035
PAGE 0 will be used to organize program sections
PAGE 1 will be used to organize data sections
Notes:
Memory blocks on F2803x are uniform (ie same
physical memory) in both PAGE 0 and PAGE 1.
That is the same memory region should not be
defined for both PAGE 0 and PAGE 1.
Doing so will result in corruption of program
and/or data.
L0 memory block is mirrored - that is
it can be accessed in high memory or low memory.
For simplicity only one instance is used in this
linker file.
Contiguous SARAM memory blocks or flash sectors can be
be combined if required to create a larger memory block.
*/
MEMORY
{
PAGE 0: /* Program Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
RAML0 : origin = 0x008000, length = 0x000800 /* on-chip RAM block L0 */
RAML1 : origin = 0x008800, length = 0x000400 /* on-chip RAM block L1 */
OTP : origin = 0x3D7800, length = 0x000400 /* on-chip OTP */
FLASHH : origin = 0x3E8000, length = 0x002000 /* on-chip FLASH */
FLASHG : origin = 0x3EA000, length = 0x002000 /* on-chip FLASH */
FLASHF : origin = 0x3EC000, length = 0x002000 /* on-chip FLASH */
FLASHE : origin = 0x3EE000, length = 0x002000 /* on-chip FLASH */
FLASHD : origin = 0x3F0000, length = 0x002000 /* on-chip FLASH */
FLASHC : origin = 0x3F2000, length = 0x002000 /* on-chip FLASH */
FLASHA : origin = 0x3F6000, length = 0x001F80 /* on-chip FLASH */
CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */
BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */
CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */
IQTABLES : origin = 0x3FE000, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3FEB50, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3FEBDC, length = 0x0000AA /* IQ Math Tables in Boot ROM */
ROM : origin = 0x3FF27C, length = 0x000D44 /* Boot ROM */
RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */
VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
/* Registers remain on PAGE1 */
BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */
RAMM0 : origin = 0x000050, length = 0x0003B0 /* on-chip RAM block M0 */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAML2 : origin = 0x008C00, length = 0x000400 /* on-chip RAM block L2 */
RAML3 : origin = 0x009000, length = 0x001000 /* on-chip RAM block L3 */
FLASHB : origin = 0x3F4000, length = 0x002000 /* on-chip FLASH */
}
/* Allocate sections to memory blocks.
Note:
codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
execution when booting to flash
ramfuncs user defined section to store functions that will be copied from Flash into RAM
*/
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHA PAGE = 0
.pinit : > FLASHA, PAGE = 0
//.text : > FLASHA PAGE = 0
.text : > FLASHA|FLASHC|FLASHE PAGE = 0 // increased this sector by combining flash sectors
codestart : > BEGIN PAGE = 0
ramfuncs : LOAD = FLASHD,
RUN = RAML0,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
RUN_START(_RamfuncsRunStart),
PAGE = 0
csmpasswds : > CSM_PWL_P0 PAGE = 0
csm_rsvd : > CSM_RSVD PAGE = 0
/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
// .ebss : > RAML2 PAGE = 1
.ebss : > RAML3 PAGE = 1
.esysmem : > RAML2 PAGE = 1
/* Initalized sections go in Flash */
/* For SDFlash to program these, they must be allocated to page 0 */
.econst : > FLASHA PAGE = 0
.switch : > FLASHA PAGE = 0
/* Allocate IQ math areas: */
IQmath : > FLASHA PAGE = 0 /* Math Code */
IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD
/* Uncomment the section below if calling the IQNexp() or IQexp()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
}
*/
/* Uncomment the section below if calling the IQNasin() or IQasin()
functions from the IQMath.lib library in order to utilize the
relevant IQ Math table in Boot ROM (This saves space and Boot ROM
is 1 wait-state). If this section is not uncommented, IQmathTables2
will be loaded into other memory (SARAM, Flash, etc.) and will take
up space, but 0 wait-state is possible.
*/
/*
IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
{
IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
}
*/
/* .reset is a standard section used by the compiler. It contains the */
/* the address of the start of _c_int00 for C Code. /*
/* When using the boot ROM this section and the CPU vector */
/* table is not needed. Thus the default type is set here to */
/* DSECT */
.reset : > RESET, PAGE = 0, TYPE = DSECT
vectors : > VECTORS PAGE = 0, TYPE = DSECT
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
DSP2803x_Device.h
//###########################################################################
//
// FILE: DSP2803x_Device.h
//
// TITLE: DSP2803x Device Definitions.
//
//###########################################################################
// $TI Release: F2803x C/C++ Header Files and Peripheral Examples V130 $
// $Release Date: May 8, 2015 $
// $Copyright: Copyright (C) 2009-2015 Texas Instruments Incorporated -
// http://www.ti.com/ ALL RIGHTS RESERVED $
//###########################################################################
#ifndef DSP2803x_DEVICE_H
#define DSP2803x_DEVICE_H
#ifdef __cplusplus
extern "C" {
#endif
#define TARGET 1
//---------------------------------------------------------------------------
// User To Select Target Device:
#define DSP28_28030PAG 0
#define DSP28_28030PN 0
#define DSP28_28031PAG 0
#define DSP28_28031PN 0
#define DSP28_28032PAG 0
#define DSP28_28032PN 0
#define DSP28_28033PAG 0
#define DSP28_28033PN 0
#define DSP28_28034PAG 0
#define DSP28_28034PN 0
#define DSP28_28035PAG 0
#define DSP28_28035PN TARGET
//---------------------------------------------------------------------------
// Common CPU Definitions:
//
extern __cregister volatile unsigned int IFR;
extern __cregister volatile unsigned int IER;
#define EINT __asm(" clrc INTM")
#define DINT __asm(" setc INTM")
#define ERTM __asm(" clrc DBGM")
#define DRTM __asm(" setc DBGM")
#define EALLOW __asm(" EALLOW")
#define EDIS __asm(" EDIS")
#define ESTOP0 __asm(" ESTOP0")
#define M_INT1 0x0001
#define M_INT2 0x0002
#define M_INT3 0x0004
#define M_INT4 0x0008
#define M_INT5 0x0010
#define M_INT6 0x0020
#define M_INT7 0x0040
#define M_INT8 0x0080
#define M_INT9 0x0100
#define M_INT10 0x0200
#define M_INT11 0x0400
#define M_INT12 0x0800
#define M_INT13 0x1000
#define M_INT14 0x2000
#define M_DLOG 0x4000
#define M_RTOS 0x8000
#define BIT0 0x0001
#define BIT1 0x0002
#define BIT2 0x0004
#define BIT3 0x0008
#define BIT4 0x0010
#define BIT5 0x0020
#define BIT6 0x0040
#define BIT7 0x0080
#define BIT8 0x0100
#define BIT9 0x0200
#define BIT10 0x0400
#define BIT11 0x0800
#define BIT12 0x1000
#define BIT13 0x2000
#define BIT14 0x4000
#define BIT15 0x8000
//---------------------------------------------------------------------------
// For Portability, User Is Recommended To Use Following Data Type Size
// Definitions For 16-bit and 32-Bit Signed/Unsigned Integers:
//
#ifndef DSP28_DATA_TYPES
#define DSP28_DATA_TYPES
typedef int int16;
typedef long int32;
typedef unsigned int Uint16;
typedef unsigned long Uint32;
typedef unsigned long int Uint64; //defiend by me
typedef float float32;
typedef long double float64;
#endif
//---------------------------------------------------------------------------
// Include All Peripheral Header Files:
//
#include "DSP2803x_Adc.h" // ADC Registers
#include "DSP2803x_BootVars.h" // Boot ROM Variables
#include "DSP2803x_DevEmu.h" // Device Emulation Registers
#include "DSP2803x_Cla.h" // Control Law Accelerator Registers
#include "DSP2803x_Comp.h" // Comparator Registers
#include "DSP2803x_CpuTimers.h" // 32-bit CPU Timers
#include "DSP2803x_ECan.h" // Enhanced eCAN Registers
#include "DSP2803x_ECap.h" // Enhanced Capture
#include "DSP2803x_EPwm.h" // Enhanced PWM
#include "DSP2803x_EQep.h" // Enhanced QEP
#include "DSP2803x_Gpio.h" // General Purpose I/O Registers
#include "DSP2803x_HRCap.h" // High Resolution Capture
#include "DSP2803x_I2c.h" // I2C Registers
#include "DSP2803x_Lin.h" // LIN Registers
#include "DSP2803x_NmiIntrupt.h" // NMI Interrupt Registers
#include "DSP2803x_PieCtrl.h" // PIE Control Registers
#include "DSP2803x_PieVect.h" // PIE Vector Table
#include "DSP2803x_Spi.h" // SPI Registers
#include "DSP2803x_Sci.h" // SCI Registers
#include "DSP2803x_SysCtrl.h" // System Control/Power Modes
#include "DSP2803x_XIntrupt.h" // External Interrupts
#if (DSP28_28035PN||DSP28_28034PN||DSP28_28033PN||DSP28_28032PN||DSP28_28031PN||DSP28_28030PN)
#define DSP28_COMP1 1
#define DSP28_COMP2 1
#define DSP28_COMP3 1
#define DSP28_EPWM1 1
#define DSP28_EPWM2 1
#define DSP28_EPWM3 1
#define DSP28_EPWM4 1
#define DSP28_EPWM5 1
#define DSP28_EPWM6 1
#define DSP28_EPWM7 1
#define DSP28_ECAP1 1
#define DSP28_EQEP1 1
#define DSP28_ECANA 1
#define DSP28_HRCAP1 1
#define DSP28_HRCAP2 1
#define DSP28_SPIA 1
#define DSP28_SPIB 1
#define DSP28_SCIA 1
#define DSP28_I2CA 1
#define DSP28_LINA 1
#endif
#if (DSP28_28035PAG||DSP28_28034PAG||DSP28_28033PAG||DSP28_28032PAG||DSP28_28031PAG||DSP28_28030PAG)
#define DSP28_COMP1 1
#define DSP28_COMP2 1
#define DSP28_COMP3 1
#define DSP28_EPWM1 1
#define DSP28_EPWM2 1
#define DSP28_EPWM3 1
#define DSP28_EPWM4 1
#define DSP28_EPWM5 1
#define DSP28_EPWM6 1
#define DSP28_EPWM7 0
#define DSP28_ECAP1 1
#define DSP28_EQEP1 1
#define DSP28_ECANA 1
#define DSP28_HRCAP1 1
#define DSP28_HRCAP2 1
#define DSP28_SPIA 1
#define DSP28_SPIB 0
#define DSP28_SCIA 1
#define DSP28_I2CA 1
#define DSP28_LINA 1
#endif
// Timer definitions based on System Clock
// 60 MHz devices
#define mSec0_5 30000 // 0.5 mS
#define mSec0_75 45000 // 0.75 mS
#define mSec1 60000 // 1.0 mS
#define mSec2 120000 // 2.0 mS
#define mSec5 300000 // 5.0 mS
#define mSec7_5 450000 // 7.5 mS
#define mSec10 600000 // 10 mS
#define mSec20 1200000 // 20 mS
#define mSec50 3000000 // 50 mS
#define mSec75 4500000 // 75 mS
#define mSec100 6000000 // 100 mS
#define mSec200 12000000 // 200 mS
#define mSec500 30000000 // 500 mS
#define mSec750 45000000 // 750 mS
#define mSec1000 60000000 // 1000 mS
#define mSec2000 120000000 // 2000 mS
#define mSec5000 300000000 // 5000 mS
#ifdef __cplusplus
}
#endif /* extern "C" */
#endif // end of DSP2803x_DEVICE_H definition
//===========================================================================
// End of file.
//===========================================================================