Part Number: TMS320F28075
Hello,
Checking the latest TRM (SPRUHM9E) and datasheet of TMS320F28075 (SPRS902G) to change the BMSP1 pin, I observed the following issues:
1) The emulator boot control register labeled EMU_BOOTCTRL in RTM and EMUBOOTCTRL in datasheet.
2) Section 4.6 of RTM, "Configuring Emulation Boot Options" refers to itself:
"The values that can be set in the BMODE field of the EMU_BOOTCTRL register are listed in Section 4.6"
3) I can not find the EMU_BOOTCTRL in the register view of CCS when connected to a device.
4) The EMU_BOOTCTRL is not listed in memory map.
5) The address 0xD00 for EMUBOOTCTRL mentioned in 6.9.1 of datasheet, but in Table 6-1 this address is the start of PieVectTable
With regards,
MHG
2)